RecipeList

The
RecipeList
item returns information about the recipes available within FactoryTalk Batch View. The
RecipeList
execute must be run once prior to advising or requesting on this item.
This table shows the input and output formats for this item.
Input and output formats
Format
Description
Input Format
Request:
RecipeList
Output Format
The RecipeList item returns in this format:
<RecipeList>
is
<RecipeInfo>
|
<RecipeInfo> <RecipeList>
<RecipeInfo>
is
<ProductVersion>
\t
<FileName>
\t
<RecipeID>
\t
<RecipeDesc>
\t
<ProductName>
\t
<ProductCode>
\t
<RecipeVersion>
\t
<RecipeVersTime>
\t
<Author>
\t
<ApprovedBy>
\t
<RecipeLevel>
\t
<RecipeType>
\t
<Abstract>
\t
<MinBatchSize>
\t
<DefBatchSize>
\t
<MaxBatchSize>
\t
<UOM>
\t
<EstDuration>
\t
<Released>
\t
<AreaModel>
\t
<AreaModelTime>
\t
<Unit>
\t
<VerifyDate>
\cr
<RecipeList>
is
<RecipeInfo>
|
<RecipeInfo> <RecipeList>
where <RecipeInfo> is
Field Name
Format
Description
<ProductVersion>
ASCII - String
The version of the product as defined in the recipe header.
<FileName>
ASCII - String
The filename of the recipe.
<RecipeID>
ASCII - String
The recipe identifier as defined in the recipe header.
<RecipeDesc>
ASCII - String
A recipe description as defined in the recipe header.
<ProductName>
ASCII - String
The product name as defined in the recipe header.
<ProductCode>
ASCII - String
The product code as defined in the recipe header.
<RecipeVersion>
ASCII - String
The recipe version as defined in the recipe header.
<RecipeVersTime>
ASCII - String dd/mm/yy hh:mm
The date/time that the recipe was saved. The format is in accordance with the date/time as set in the Control Panel.
<Author>
ASCII - String
The recipe author as defined in the recipe header.
<ApprovedBy>
ASCII - String
The approved by name as defined in the recipe header.
<RecipeLevel>
ASCII - String
The level of the recipe: PROCEDURE, UNIT PROCEDURE, or OPERATION.
<RecipeType>
ASCII - String
The type of equipment requirements for the recipe: CLASS or INSTANCE.
<Abstract>
ASCII - String
The recipe abstract as defined in the recipe header.
<MinBatchSize>
ASCII - String
The minimum batch size, as defined in the recipe header.
<DefBatchSize>
ASCII - String
The default batch size, as defined in the recipe header.
<MaxBatchSize>
ASCII - String
The maximum batch size, as defined in the recipe header.
<UOM>
ASCII - String
The unit of measure, as defined in the recipe header.
<EstDuration>
ASCII - String
The estimated duration of the batch, as defined in the recipe header.
<Released>
ASCII - String
Indicates if the recipe has been released to production. Always TRUE. (Only recipes which have been released to production are included in the RecipeList item.)
<AreaModel>
ASCII - String
The area model file and path name against which the recipe was verified.
<AreaModelTime>
dd/mm/yy hh:mm
The date/time of area model file against which the recipe was verified. The format will be in accordance with the date/time as set in the Control Panel.
<Unit>
ASCII - String
The name of the unit or alias to which the recipe is bound. Will return an empty string for PROCEDURE level recipes.
<VerifyDate>
ASCII - String dd/mm/yy hh:mm
The latest modification date/time for the recipe. The format will be in accordance with the date/time as set in the Control Panel.
This is an example of the return on this request.
Example
: A request on
object.GetItem(RecipeList)
could return:
3.0 \t FRENCH_VANILLAPREMIUM1_MEGA_PARLOR_OPT_2_U1.UPC \t FRENCH_VANILLAPREMIUM1_MEGA_PARLOR_OPT_2_U1 \t French Vanilla IceCream \t French Vanilla \t FVP-101 \t Premium 1 \t 2/24/2022 10:11:33 AM \t Administrator \t rpmServer (STAGE1\rpmServer) on computer STAGE1 \t UNIT PROCEDURE \t Instance \t The general recipe French_Vanilla, Variant= Premium, Version= 1 is successfully converted to master recipe FRENCH_VANILLAPREMIUM1_MEGA_PARLOR \t 25 \t 50 \t 100 \t KG \t \t TRUE \t \\STATION5\PROGRAM FILES\ROCKWELL SOFTWARE\BATCH\SAMPLEAPP\RECIPES\ICE_CREAM.CFG \t 2/24/2022 10:05:16 AM \t MP_MIXERFREEZER1 \t 2/24/2022 10:11:27 AM \crlf
...
3.0 \t CLS_STRAWBERRY_ICEMILK.BPC \t CLS_STRAWBERRY_ICEMILK \t Strawberry Ice Milk - Reduced Fat Ice Cream - class based \t Strawberry Ice Milk \t SIM-101 \t 1.0 \t 2/24/2022 10:11:34 AM \t Mark Shepard \t MSS \t PROCEDURE \t Class \t \t 3000 \t 5000 \t 7000 \t KG \t 45 \t TRUE \t \\STATION5\PROGRAM FILES\ROCKWELL SOFTWARE\BATCH\SAMPLEAPP\RECIPES\ICE_CREAM.CFG \t 2/24/2022 10:05:16 AM \t \t 2/24/2022 10:11:27 AM \crlf
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal