ErrorMessage

The
ErrorMessage
item returns the most recent severe message in the
FactoryTalk Batch
Server’s log file.
This table shows the input and output formats for this item.
Input and output formats for this item
Format
Description
Input Format
Request:
ErrorMessage
Output Format
The ErrorMessage item returns in this format:
<Time>
\t
<Description>
\t
<Additional Data>
\crlf
Field Name
Format
Description
<Time>
ASCII – String
Time when the message generated.
<Description>
ASCII – String
General message description.
<Additional Data>
ASCII – String
More specific message information. May be <NullString> or a blank space character <sp>.
This is an example of the return on this request.
A request on
object.GetItem(ErrorMessage)
could return:
2022.02.24 16:14:49:220 \t SETTING CONVERSATION STATUS BAD \t SERVER:OPC_SIM \crlf
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal