DDEClientCount

The
DDEClientCount
item returns the number of DDE clients connected to the
FactoryTalk Batch
Server.
This table shows the input and output formats for this item.
Input and output formats for this item
Format
Description
Input Format
Request:
DDEClientCount
Output Format
The DDEClientCount item returns in this format:
<DDECount>
Field Name
Format
Description
<DDECount>
ASCII - String
Number of DDE clients connected to the
FactoryTalk Batch
Server.
This is an example of the return on this request.
A request on the
object.GetItem(DDEClientCount)
could return:
1
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal