DataServerStatistics

The
DataServerStatistics
item returns a detailed description of each configured data server conversation and each conversation’s status.
This table shows the input and output formats for this item.
Input and output formats for this item
Format
Description
Input Format
Request:
DataServerStatistics
Output Format
The DataServerStatistics item returns in this format:
<Statistics>
is
<NullList>
|
<ServerList>
<ServerList>
is
<ServerRecord>
|
<ServerRecord>
<ServerList>
<ServerRecord>
is
<ServerName>
\t
<ConfigString1>
\t
<ConfigString2>
\t
<ConversationStatus>
\t
<WatchDog>
\crlf
where <ServerRecord> is:
Field Name
Format
Description
<ServerName>
ASCII - String
Data server name.
<ConfigString1>
ASCII - String
Protocol-specific configuration string exposed:
OPC: Data Server brand name from DSDF file.
CIP: The string constant "FactoryTalk Linx".
FTD:The Area Path used in establishing a connection to the
FactoryTalk
Live Data server.
<ConfigString2>
ASCII - String
Protocol-specific configuration string exposed:
OPC: Data server’s configured watchdog read item access path.
CIP: Controller path
FTD: Data server’s configured watchdog read item access path.
<Conversation Status>
ASCII – String
Language-specific word for the current conversation status between the
FactoryTalk Batch
Server and the data server:
Good, Bad, Suspect, or Lost
<WatchDog>
ASCII – String
Protocol-specific configuration string exposed:
OPC: Data server’s configured watchdog read item name.
CIP: Unused (<sp>)
FTD: Data server’s configured watchdog read item name.
This is an example of the return on this request.
TIP:
A request on the
object.GetItem(DataServerStatistics)
could return this for two servers:
OPC_SIM \t \t PHASES \t GOOD \t WATCHDOG \crlf
INSTRUCTIONBASEDSERVER \t \t INSTRUCTIONS \t GOOD \t WATCHDOG \crlf
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal