CreateIDBatchStepDataList

The
CreateIDBatchStepDataList
item returns a list of all the steps in a recipe batch, and each step’s status.
This table shows the input and output formats for this item.
Input and output formats for this item
Format
Description
Input Format
Request:
CreateIDBatchStepDataList
CreateID
is
ASCII – Integer, INTERNAL identifier assigned by the
FactoryTalk Batch
Server to a batch when it is created. Obtained from the
BatchList
item.
Output Format
The CreateIDBatchStepDataList item returns in this format:
<BSList>
is
<NullList>
|
<StepList>
<StepList>
is
<Step>
\crlf |
<Step>
\crlf
<StepList>
<Step>
is
<ID>
\t
<Name>
\t
<SP88Type>
\t
<KeyPName>
\t
<KeyValue>
\t
<State>
\t
<Mode>
\t
<UnitName>
\t
<Control>
\t
<Index>
\t
<Paused>
\t
<Msg>
\t
<Rqst>
\t
<Fail>
\t
<ParmList>
\t
<RepParmList>
\t
<OwnerID>
\t
<OwnerName>
\t
<CmdMask>
where:
Field Name
Format
Description
<ID>
ASCII - Integer
Element ID (defined by ProcedureIDData item)
<Name>
ASCII - String
Element Name
<SP88Type>
ASCII - Integer
Step type:
  • 0 = Null
  • 1 = Procedure
  • 2 = Unit Procedure
  • 3 = Operation
  • 4 = Phase
<KeyPName>
ASCII - String
Key Parameter Name: may contain a single space if the step does not have a key parameter value.
<KeyValue>
ASCII - String
Step’s Key Value: may contain a single space if the step does not have a key parameter value.
<State>
ASCII - String
Element State
<Mode>
ASCII - String
Step’s Mode:
  • O-AUTO
  • P-AUTO
  • S-AUTO
  • MANUAL
  • UNKNOWN
<UnitName>
ASCII - String
Unit under which the Step runs.
<Control>
ASCII - String
Who controls the Step:
  • NONE
  • PROGRAM
  • EXTERNAL
This field may contain a single space character if the step is not an active recipe element.
<Index>
ASCII - Integer
Step Index: the value may be a single-space character if the step is not an active recipe element.
<Paused>
ASCII - Integer
Indicates if the step is Paused.
  • 0 = False
  • 1 = True
Only a Phase can have Paused = True. All others are False.
<Msg>
ASCII - String
Step Message
<Rqst>
ASCII - Integer
Step Request, contents of request register
<Fail>
ASCII- String
Fail Message, single space if not active or no failures
<ParmList>
Variable list
List of recipe parameters
<RepParmList>
Variable list
List of report parameters
<OwnerID>
ASCII - Integer
Element Owner ID, single space if step not of phase
<OwnerName>
ASCII - String
Owner Name, single space if step not of phase
<CmdMask>
ASCII - Integer
Command masks
where <KeyValue> is:
<KeyValue>
is
<ValueAndEU>
|
<EquipmentID>
<ValueAndEU>
is
<DefaultValue>
<sp>
<EngUnits>
where <ValueAndEU> is:
Field Name
Format
Description
<EquipmentID>
ASCII – String
Unique ID corresponding to the step.
<DefaultValue>
ASCII – String
Default value of display parameter
<EngUnits>
ASCII – String
Engineering units associated with default value
where <ParmList> is:
<ParmList>
is
$PARM \t
<Parameters>
\t $END
<Parameters>
is
<NullList>
|
<PList>
<PList>
is
<Parameter>
|
<Parameter>
\t
<PList>
<Parameter>
is
<ParmName>
\t
<Value>
Field Name
Format
Description
<ParmName>
ASCII – String
Parameter Name
<Value>
ASCII – String
Current batch value.
???
indicates that there is no value assigned.
where <RepParmList> is:
<RepParmList>
is
$REPORT \t
<Parameters>
\t $END
<Parameters>
is
<NullList>
|
<RList>
<RList>
is
<Parameter>
|
<Parameter>
\t
<RList>
<Parameter>
is
<ParmName>
\t
<Value>
Field Name
Format
Description
<ParmName>
ASCII – String
Report Parameter Name
<Value>
ASCII – String
Current batch value
This is an example of the return on this request.
TIP:
The BatchList contains a batch with the CreateID of 21. Use this Request to see a list of steps for this batch: object.GetItem(21BatchStepDataList), which could return:
627 \t BATCH_ID \t 3 \t \t MP_MIXERFREEZER2 \t RUNNING \t O_AUTO \t MP_MIXERFREEZER2 \t PROGRAM \t \t 0 \t \t \t \t $PARM \t \t $END \t $REPORT \t \t $END \t \t \t 2087 \crlf
661 \t MBR_ADD:1 \t 4 \t \t \t \t \t MP_MIXERFREEZER2 \t \t 0 \t \t \t \t \t $PARM \t MATERIAL \t SUGAR_GRANULATED \t AMOUNT \t 800 \t $BINDCONTAINER \t NULL_CONTAINER \t $BINDEQMODULE \t \t $END \t $REPORT \t ACTUAL_AMOUNT \t 700 \t FEED_COMPLETE \t YES \t $END \t \t \t 262144\n662 \t AGITATE:1 \t 4 \t \t \t \t \t MP_MIXERFREEZER2 \t \t 0 \t \t \t \t \t $PARM \t SPEED_RATE \t 5 \t $END \t $REPORT \t MIX_SPEED \t 30 \t $END \t \t \t 0 \crlf
632 \t MBR_ADD:2 \t 4 \t \t \t \t \t MP_MIXERFREEZER2 \t \t 0 \t \t \t \t \t $PARM \t MATERIAL \t EGG_YOLK \t AMOUNT \t 180 \t $BINDCONTAINER \t NULL_CONTAINER \t $BINDEQMODULE \t \t $END \t $REPORT \t ACTUAL_AMOUNT \t 150 \t FEED_COMPLETE \t YES \t $END \t \t \t 262144\n636 \t MBR_ADD:3 \t 4 \t \t \t \t \t MP_MIXERFREEZER2 \t \t 0 \t \t \t \t \t $PARM \t MATERIAL \t CREAM \t AMOUNT \t 2000 \t $BINDCONTAINER \t NULL_CONTAINER \t $BINDEQMODULE \t \t $END \t $REPORT \t ACTUAL_AMOUNT \t 2000 \t FEED_COMPLETE \t YES \t $END \t \t \t 262144 \crlf
660 \t TEMP_CTL:1 \t 4 \t \t \t \t \t MP_MIXERFREEZER2 \t \t 0 \t \t \t \t \t $PARM \t HOLD_TIME \t 5 \t TEMP_SP \t 71.1 \t $END \t $REPORT \t TEMPERATURE \t 0 \t TIME_HELD \t 0 \t $END \t \t \t 0 \crlf
659 \t AGITATE:2 \t 4 \t \t \t \t \t MP_MIXERFREEZER2 \t \t 0 \t \t \t \t \t $PARM \t SPEED_RATE \t 5 \t $END \t $REPORT \t MIX_SPEED \t 30 \t $END \t \t \t 0 \crlf
658 \t MBR_ADD:4 \t 4 \t \t \t \t \t MP_MIXERFREEZER2 \t \t 0 \t \t \t \t \t $PARM \t MATERIAL \t MILK \t AMOUNT \t 2000 \t $BINDCONTAINER \t NULL_CONTAINER \t $BINDEQMODULE \t \t $END \t $REPORT \t ACTUAL_AMOUNT \t 2000 \t FEED_COMPLETE \t YES \t $END \t \t \t 262144\n640 \t AGITATE:3 \t 4 \t \t \t \t \t MP_MIXERFREEZER2 \t \t 0 \t \t \t \t \t $PARM \t SPEED_RATE \t 5 \t $END \t $REPORT \t MIX_SPEED \t 30 \t $END \t \t \t 0 \crlf
644 \t MBR_ADD:5 \t 4 \t \t \t RUNNING \t P_AUTO \t MP_MIXERFREEZER2 \t PROGRAM \t 10 \t 0 \t \t 0 \t \t $PARM \t MATERIAL \t VANILLA \t AMOUNT \t 20 \t $BINDCONTAINER \t TEMPFLAVOR_VANILLA \t $BINDEQMODULE \t MP_ADDFLAVOR_MF2 \t $END \t $REPORT \t ACTUAL_AMOUNT \t \t FEED_COMPLETE \t \t $END \t -1142 \t 21:FRENCH_VANILLAPREMIUM1_MEGA_PARLOR_OPT_1_O1 \t 32 \crlf
TIP: Continued
657 \t TEMP_CTL:2 \t 4 \t \t \t \t \t MP_MIXERFREEZER2 \t \t 0 \t \t \t \t \t $PARM \t HOLD_TIME \t 5 \t TEMP_SP \t 71.1 \t $END \t $REPORT \t TEMPERATURE \t \t TIME_HELD \t \t $END \t \t \t 0\n648 \t RECIRC:1 \t 4 \t \t \t \t \t MP_MIXERFREEZER2 \t \t 0 \t \t \t \t \t $PARM \t RECIRC_RATE \t 50 \t $END \t $REPORT \t FINAL_RECIRC_RATE \t \t $END \t \t \t 0\n652 \t MBR_DUMP:1 \t 4 \t \t \t \t \t MP_MIXERFREEZER2 \t \t 0 \t \t \t \t \t $PARM \t MATERIAL \t IC_FRENCH_VANILLA \t AMOUNT \t -5000 \t $BINDCONTAINER \t \t $BINDEQMODULE \t \t $END \t $REPORT \t ACTUAL_AMOUNT \t \t FEED_COMPLETE \t \t $END \t \t \t 262144 \crlf
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal