BLRecipe_x

The
BLRecipe_x
item returns the recipe for the
x
th batch in the batch list.
This table shows the input and output formats for this item.
Input and output formats
Format
Description
Input Format
Request: BLRecipe_
<RowNumber>
<RowNumber>
is
ASCII - Integer
An array index. When an unacknowledged prompt generates, it adds to an array. If the unacknowledged prompts list is not sorted, then
x
is the row number of the unacknowledged prompt appearing in the unacknowledged prompts list.
The BLRecipe_x item requires this setting in the
FactoryTalk Administration Console
FactoryTalk Batch Services Properties
Advanced
tab:
MaxBatchTableLength = n
where
n
is the maximum number of batches accessible to this Item (the maximum number of entries in the array). If the number of batches in the batch list is larger than
n
, then this item will only access the first
n
batches in a non-sorted batch list. When a batch with an index of less than
n
is removed from the batch list, all subsequent batches will have their index decreased by one. The default value of
MaxBatchTableLength
is
0
(zero).
Output Format
The BLRecipe_x item returns in this format:
<RecipeName>
Field Name
Format
Description
<RecipeName>
ASCII – String
Name of the batch appearing on
x
th row of the batch list.
This table is an example of a typical batch list containing three batches with batch IDs BATCH_98, BATCH_99, and BATCH_100:
Batch list example
Batch ID
Recipe
Desc
Start Time
State
Mode
BATCH_98
Vanilla
Ice Cream 1
2/24/2022 1:22:02 pm
RUNNING
O_Auto
BATCH_99
Chocolate
Ice Cream 2
2/24/2022 1:24:12 pm
RUNNING
S_Auto
BATCH_100
Premium French Vanilla
Ice Cream 3
2/24/2022 1:32:30 pm
RUNNING
O_Auto
This is an example of the return on this request.
TIP:
A request on
object
.
GetItem(BLRecipe_3)
would return the recipe name of the batch in the batch list's third row:
Premium French Vanilla
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal