SignoffSignature
The
SIGNOFFSIGNATURE
execute allows a client to sign a signature request on an incomplete signature, excluding those generated by private interfaces.The format and return for this execute includes:
Execute Format | A FactoryTalk Batch Server supports an execute with this format:[SIGNOFFSIGNATURE( Item, UserID, SignatureID, SignoffNumber, Domain, Comment, SignerID, Password )] | |
|---|---|---|
where: | Item | Response item name as specified by the client. |
UserID | User Identification entered into the event journal associated with this event. | |
SignatureID | Unique ID of the signature for which the signoff is intended. | |
SignoffNumber | Signoff number for which the signoff is intended
(1 or 2). | |
Comment | Comment string being passed with signoff. The locale-specific list separator character should be escaped from the comment argument as follows: The client application shall replace all instances of the
‘/’ character with ‘/FS’. The client application shall then replace all instances of the list separator character with ‘/LS’. The tab character shall be considered illegal for the comment argument. If a tab character is detected in the comment string, the execute shall fail. | |
Domain | Domain to be used when authenticating the SignerID parameter. | |
SignerID | Security-related User ID of the user attempting the signoff (not the full name). | |
Password | Security-related password of the User attempting the signoff. | |
Action | A successful SIGNOFFSIGNATURE fulfills a signoff on an incomplete signature. | |
Return Format | The response item populates with this data: SUCCESS: <ActionID> | FAIL: <message> Where action ID = integer value; the Action ID of the action that required the signature. (Only the final sign-off of a Signature returns an Action ID.) | |
where: | ||
Field | Format | Description |
<ActionID> | ASCII – Integer | Action identifier associated with signature(s) generated as a result of the potential parameter value change. The parameter value will not actually change unless all signatures are successfully signed. |
<message> | ASCII - String | Error message appropriately formatted for operator display. |
The following is an example of the return on this execute.
An execute string consisting of:
SIGNOFFSIGNATURE(Item,Station2/View,993,1,Italy,What is this,LDVinci,
helicopter)
Could return:
SUCCESS: or SUCCESS:Action ID
Provide Feedback