Parms
The
PARMS
execute obtains the parameters of a procedure.The format and return for this execute includes:
Execute Format | A FactoryTalk Batch Server supports an execute string with the PARMS keyword. The format of the execute string:[PARMS( Item,UserID,ProcedureID )] | |
|---|---|---|
where: | Item | Item name as specified by the client. |
UserID | User identification associated with this event. | |
ProcedureID | Unique path name to the procedure, starting with the CreateID and followed by the step name(s), all of which are tab delimited. | |
Action | A successful PARMS execute returns the parameter string into the item specified by the client. | |
Return Format | The PARMS execute s returns in this format: <Parameter> \t <ResponseType> \t <EngUnits> \t <MaxValue> \t <MinValue> \t <Value> \crlf | |
where: | ||
Field Name | Format | Description |
<Parameter> | ASCII - String | Parameter name required to create the batch. |
<ResponseType> | ASCII - Integer | Data type for the response:
|
<EngUnits> | ASCII - String | Engineering units for the parameter. |
<MaxValue> | ASCII - String | High range for the parameter. |
<MinValue> | ASCII - String | Low range for the parameter. |
<Value> | ASCII - String | Current value of the parameter. |
The following is an example of the return on this execute.
An execute string consisting of:
[PARMS(Item,UserID,41 \t CLS_SWEETCREAM_UP:1 \t CLS_SWEETCREAM_OP:1 \t
TEMP_CTL:1)
Could place this data in Item for the client:
HOLD_TIME \t 1 \t MINUTES \t 60 \t 0 \t 5 \crlf
TEMP_SP \t 1 \t DEG \t C \t 100 \t 0 \t 71.1 \crlf
Provide Feedback