Mtrl_Info

The
MTRL_INFO
execute returns the information necessary allowing material selection for a
Material Manager
phase written as material class-based.
The format and return for this execute includes:
Format and return
Execute Format
A
FactoryTalk Batch
Server supports an execute with this format:
[MTRL_INFO(
Item,UserID,RecipeFileName
)]
where:
Item
Item name as specified by the client.
UserID
User identification associated with this event.
RecipeID
Recipe filename.
Action
A MTRL_INFO execute returns necessary information to select materials for
Material Manager
phases that have a MATERIAL_CLASS parameter set to a non-NULL_CLASS value.
Return Format
The MTRL_INFO execute returns in this format:
SUCCESS:
<Phase-MaterialInfo>
| FAIL:
<Message>
where:
<Phase-MaterialInfo>
is
<Null List>
|
< Phase-Material List>
<Phase-MaterialList>
is
<Phase-Material Record>
|
<Phase-Material Record>
\crlf
< Phase-Material List>
<Phase-MaterialRecord>
is
<Phase Pathname>
\t
<Material Class Name>
\t
<Material List>
$END
<MaterialList>
is
< Material Name>
|
< Material Name>
\t
<Material List>
where:
Field Name
Format
Description
<Phase Pathname>
ASCII
Full recipe pathname to the phase. (for example, PROC_1\UNITPROC_1:1\OPER_1:3\ADD:4)
<MaterialClass Name>
ASCII
Name of material class referenced by the MATERIAL_CLASS parameter. (for example, SWEETENER)
<MaterialName>
ASCII
Name of a material of the designated material class. (for example, RAW_SUGAR)
TIP:
"SUCCESS:" followed by a null list indicates that no material class references exist to be resolved.
"
SUCCESS:" followed by a non-null list implies that all Material Lists returned must also be non-empty. If an empty Material List would have resulted (that is, no Material to choose for the Material Class), MTRL_INFO returns "FAIL:".
The following is an example of the return on this execute.
An execute string consisting of:
MTRL_INFO (Item,User,VANILLA_ICE_CREAM.BPC)
Could return:
SUCCESS:YUMMY_STUFF\SWEETCREAM_UP:1\SWEETCREAM_OP:2\ADD:1\tSWEETENERS\tRAW_SUGAR\tBROWN_SUGAR\tSYRUP$END\crlf
YUMMY_STUFF\CHOCOLATE_UP:1\CHOCOLATE_OP:2\ADD:1\tDARK_CHOCOLATES\t68_PER_CENT_COCOA\t52_PER_CENT_COCOA$END
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal