GetPossibleLegalUnits
The
GETPOSSIBLELEGALUNITS
execute retrieves the possible binding options for a non-statically bound unit procedure or operation.The format and return for this execute includes:
Execute Format | A FactoryTalk Batch Server supports an execute with this format:[GETPOSSIBLELEGALUNITS( Item, UserID,CreateID \t UnitProcName )] | ||
|---|---|---|---|
where: | Item | Name of the response item as specified by the client. | |
UserID | User Identification entered into the event journal associated with this
event. | ||
CreateID | Unique ID, as assigned by the system, of the procedure which contains the step which requires binding | ||
UnitProcName | Path to a step representing a Unit Procedure inside of a Batch Procedure.
<Path> | ||
where: | |||
<Path> | is | <CreateID> /t <StepIdentifier> | |
where: | |||
Field | Format | Description | |
<CreateID> | ASCII - Integer | Unique batch ID assigned by the FactoryTalk Batch Server. | |
<StepIdentifier> | ASCII – String | Step identifier (for example, Mix:1) | |
Action | A successful GETPOSSIBLELEGALUNITS execute returns the alias name along with a list of IDs and names of the possible binding units or binding options for the specified Unit Procedure or Operation. | ||
Return Format | The response item populates with this data: SUCCESS:[ <Units> ] | FAIL:<message> | FAILED | ||
<Units> | is | <UnitAlias>,<UnitList> | |
<UnitList> | is | <Unit> | <Unit>,<UnitList> | |
<Unit> | is | <UnitName>,<UnitID> | |
where: | |||
Field Name | Format | Description | |
<UnitAlias> | ASCII - String | Alias associated with the specified Unit Procedure. | |
<UnitName> | ASCII - String | Name of a Unit that can be a legal bind target for the Unit Procedure, or a legal binding option (Prompt or First Available) | |
<UnitID> | ASCII - String | Unit ID associated with the unit name. The legal binding options have this associated Unit ID:
| |
The following is an example of the return on this execute.
An execute string consisting of:
GETPOSSIBLELEGALUNITS(Item,Station2/View,36 \t ADDCREAM_UP:1)
Could return:
SUCCESS:MIXER,NP_MIXER1,55,NP_MIXER2,84,PROMPT,-1,FIRST AVAILABLE,-2
Provide Feedback