GetLegalUnits

The
GETLEGALUNITS
execute retrieves the legal binding options for a non-statically bound unit procedure or operation.
The format and return for this execute includes:
Format and return
Execute Format
A
FactoryTalk Batch
Server supports an execute with this format:
[GETLEGALUNITS(
Item,UserID,CreateID \t UnitProcName
)]
where:
Item
Item name as specified by the client.
UserID
User identification associated with this event.
CreateID
Procedure’s unique ID, as assigned by the system, which contains the step that requires binding.
UnitProcName
Path to a step representing a Unit Procedure inside of a Batch Procedure.
<Path>
where:
<Path>
is
<CreateID>
/t
<StepIdentifier>
where:
Field
Format
Description
<CreateID>
ASCII - Integer
Unique batch ID assigned by the
FactoryTalk Batch
Server.
<StepIdentifier>
ASCII – String
Step identifier (for example, Mix:1)
Action
A successful GETLEGALUNITS execute returns the alias name along with a list of IDs and legal binding unit names or binding options for the specified unit procedure or operation.
Return Format
The item populates with this data:
SUCCESS:[
<Units>
] | FAIL:<message> | FAILED
<Units>
is
<UnitAlias>,<UnitList>
<UnitList>
is
<Unit>
|
<Unit>,<UnitList>
<Unit>
is
<UnitName>,<UnitID>
where:
Field Name
Format
Description
<UnitAlias>
ASCII - String
Alias associated with the specified unit procedure.
<UnitName>
ASCII - String
Unit name to which the procedure may be bound, or a legal binding option (Prompt or First Available).
<UnitID>
ASCII - String
Unit ID associated with the unit name. The legal binding options have this associated Unit ID:
Prompt = -1
First Available = -2
The following is an example of the return on this execute.
An execute string consisting of:
GETLEGALUNITS(LegalUnits,UserID,36 \t MCLS_SWEETCREAM_UP:1)
Could place this data in the item LegalUnits for the client:
SUCCESS:MIXER,NP_MIXER1,55,NP_MIXER2,84,PROMPT,-1,FIRST AVAILABLE,-2,
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal