GetLegalEqModules

The
GETLEGALEQMODULES
execute retrieves a list of phase-container-lot entries to be considered for manually binding or rebinding a phase step.
The format and return for this execute includes:
Format and return
Execute Format
A
FactoryTalk Batch
Server supports an execute with this format:
[GETLEGALEQMODULES(
Item,UserID,PhaseName
)]
where:
Item
Item name as specified by the client.
UserID
User identification associated with this event.
PhaseName
Unique hierarchical path name to the phase:
Procedure Level: CreateID \t ProcedureName \t UnitProcName \t OperName \t PhaseName
Unit Procedure Level: CreateID \t UnitProcName \t OperName \t PhaseName
Operation Level: CreateID \t OperName \t PhaseName
Action
A successful GETLEGALEQMODULES execute returns the alias name along with a list of names of the legal binding phase-container-lot entries for a phase step’s manual binding or rebinding.
Return Format
The item populates with this data:
SUCCESS:[
<StepData>, <EqModuleList>,<UseAutoBind>
] | FAIL:
<message>
where:
<StepData>
is
<Material>,<Amount>,<MaterialEU>,<FeedType>
<EqModuleList>
is
<EqModule>
|
<EqModule>,<EqModuleList>
<EqModule>
is
<EqModuleName>
,
<ContainerName>, <Capacity>
,
<ContainerEU>
,
<LotName>, <Label>
<UseAutoBind>
is
"AUTOMATIC,,0,,,,PROMPT,,0,,,,"
where:
Field Name
Format
Description
<Material>
ASCII-String
Material name from the phase’s MATERIAL parameter.
<UseAutoBind>
ASCII-String
Data passed to client applications permitting the operator to manually instruct the phase to use Automatic Phase Binding.
<Amount>
ASCII-Integer
Material quantity to process from the phase’s AMOUNT parameter. This value is positive for a material addition and negative for a material distribution.
<MaterialEU>
ASCII-String
Engineering units for measuring the quantities of material.
<FeedType>
ASCII-String
String "ADD" or "DUMP"
<EqModule
Name>
ASCII-String
Phase name that could be selected for binding.
<ContainerName>
ASCII-String
Container name that could be selected for binding.
<Capacity>
ASCII-String
Material Addition: Material quantity available in the container.
Material Distribution: Remaining storage capacity in a container.
<ContainerEU>
ASCII-String
Engineering units for measuring a container’s volume.
<LotName>
Name of the lot assigned to a specific material sublot in a container (if defined or known) - could be blank.
<Label>
String label assigned to a sublot (if defined or known) - could be blank.
The following is an example of the return on this execute.
An execute string consisting of:
GETLEGALEQMODULES(Item, Station5\Operator,42 \t MCLS_SWEETCREAM_UP:1 \t MCLS_SWEETCREAM_OP:1 \t MBR_ADD:2)
Requesting data from Item could return:
SUCCESS:EGG_YOLK,750,KG,ADD,NP_ADDSWEET_M1,SUGAR_SHACK1,66625366,KG,SUGARCANELOT3, ,AUTOMATIC, ,0, , , ,PROMPT, ,0, , , ,
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal