ControlStrategy

The
CONTROLSTRATEGY
execute returns a list of control strategies configured for the specified phase.
The format and return for this execute includes:
Format and return
Execute Format
A
FactoryTalk Batch
Server supports an execute with this format:
[CONTROLSTRATEGY(
Item,UserID,PhaseID
)]
where:
Item
Item name as specified by the client.
UserID
User identification associated with this event.
PhaseID
Equipment ID for the phase as configured in
FactoryTalk Batch Equipment Editor
.
Action
A successful CONTROLSTRATEGY execute results in a list of control strategies configured for the specified phase.
Return Format
The item populates with this data:
<ControlStrategyResponse>
is
SUCCESS:
<sp><ControlStrategyData>
|
FAIL:
<message>
| FAILED
<ControlStrategyData>
is
<NullList>
\crlf |
<ControlStrategyList>
<ControlStrategyList>
is
<ControlStrategy>
\crlf |
<ControlStrategy>
\crlf
<ControlStrategyList>
<ControlStrategy>
is
<CStrategyID>
\t
<CStrategyName>
Field Name
Format
Description
<CStrategyID>
ASCII - Integer
ID assigned to the control strategy.
<CStrategy
Name>
ASCII - String
Name assigned to the control strategy.
The following is an example of the return on this execute.
An execute string:
[CONTROLSTRATEGY(Item,UserID,68)]
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal