CancelSignature

The
CANCELSIGNATURE
execute allows a client to cancel a signature request on an incomplete signature, excluding those that were generated by private interfaces.
The format and return for this execute includes:
Format and return
Execute Format
A
FactoryTalk Batch
Server supports an execute with this format:
[CANCELSIGNATURE(
Item, UserID, SignatureID
)]
where:
Field
Format
Description
Item
ASCII - String
Name of the response item, as specified by the client.
UserID
ASCII - String
User Identification entered into the event journal associated with this event.
SignatureID
ASCII - Integer
Unique ID of the signature to be cancelled.
Action
A successful CANCELSIGNATURE request cancels the specified signature if it is in the incomplete state and not generated by a private interface.
Return Format
The response item populates with this data:
SUCCESS: | FAIL:
<message>
where:
Field
Format
Description
<message>
ASCII - String
Error message appropriately formatted for operator display.
The following is an example of the return on this execute.
An execute string consisting of:
CancelSignature(Item,Station2/View,993)
Could return:
SUCCESS:
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal