AutoRemove

The
AUTOREMOVE
execute tells the server to automatically remove a batch when its state reaches complete or cancels a previous
AUTOREMOVE
execute.
The format and return for this execute includes:
Format and return
Format
Description
Execute Format
A
FactoryTalk Batch
Server supports an execute string with the AUTOREMOVE keyword. The format of the execute string:
[AUTOREMOVE(
ResponseItem, UserID, CreateID, AutoRemove
)]
where:
ResponseItem
Name of the response item.
UserID
User identification associated with this event.
CreateID
Create ID of the batch to automatically remove.
AutoRemove
ON to automatically remove the batch; OFF to allow the batch to stay on the batch list.
Action
A successful AUTOREMOVE (... ON) execute causes the
FactoryTalk Batch
Server to remove the batch when its state reaches COMPLETE. A successful AUTOREMOVE (... OFF) execute does not allow the server to remove the batch without a REMOVE execute.
Return Format
SUCCESS: | FAIL:
<message>
TIP:
When Electronic Signatures are enabled and a Remove Command Verification Policy is configured in the area model, then all
AUTOREMOVE
executes sent to the
FactoryTalk Batch
Server fail and an appropriate error message displays.
The following is an example of the return on this execute.
An execute string:
[AUTOREMOVE(Item_1,operator,17,on)]
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal