AddEvent
The
ADDEVENT
execute allows an external application to append an event in one or all active FactoryTalk Batch
electronic batch record files based on the BatchID.The format and return for this execute includes:
Format | Description | |
|---|---|---|
Execute Format | A FactoryTalk Batch Server supports an execute with this format:[ADDEVENT( Item,UserID,BatchID,Type,Desc,Value,EU,Cell,Unit,Phase )] | |
where: | ||
Item | Item name as specified by the client. | |
UserID | User ID entered into the event journal with this event. | |
BatchID | Operator entered batch identification. Use ‘*’ to place the event information into all open electronic batch records. | |
Type | Type of event being added. | |
Desc | Description of the event being added. | |
Value | Value of the event being added. | |
EU | (optional) Engineering units associated with the event. | |
Cell | (optional) Process cell which is associated with the event. | |
Unit | (optional) Unit which is associated with the event. | |
Phase | (optional) Phase associated with the event. | |
Action | A successful ADDEVENT FactoryTalk Batch Server automatically completes these fields: TIME, AREA, RECIPE, PHASE_DESC, and UNIQUE_ID. If, however, the event is targeted at a single batch, and the batch product is configured for signature confirmation of "comments", then the addition of the event record to the event journal is queued pending a successful signature request signoff. | |
Return Format | The item populates with this data: SUCCESS: | SUCCESS: <ActionID> | FAIL: <message> | |
where: | ||
Field | Format | Description |
<ActionID> | ASCII – Integer | Action ID associated with signature(s) generated as a result of the potential prompt response. The prompt response is not actually processed unless all signature requests are successfully signed off. |
<message> | ASCII - String | Error message appropriately formatted for operator display. |
The following is an example of the return on this execute.
An execute string consisting of:
[ADDEVENT(Item,Station5\Operator,Batch_100,Comment,OperatorComment,This is a
comment)]
Could return:
SUCCESS:997
Provide Feedback