Modify event log settings
To prevent the system event logs from exceeding the maximum allowable size, configure the application and system log to overwrite events as needed.
To modify event log settings:
- Navigate toControl Panel > Administrative Tools > Event Viewer.
- Right-clickApplication, and then selectProperties. TheApplication Propertiesdialog box opens.
- In theLog sizearea, selectOverwrite events as needed,and then selectOK.
- Repeat steps 2 and 3 for theSystem.
- Exit theEvent Viewer.
Provide Feedback