Perform incremental archiving

Use
Incremental Archiving
to defer control of batch archiving to
FactoryTalk® Event Archiver
and to perform batch reporting at user-defined intervals during batch execution. Specify the incremental period between active archiving in
Minutes
or
Seconds
. The minimum setting is 5 seconds or 1 minute. The maximum is 9999 minutes. Setting the value outside of this range causes
FactoryTalk Event Archiver
to run in 5 minute incremental periods.
To update the incremental period after making changes, stop and restart the
FactoryTalk Event Archiver
service.
Configure the Incremental Archiving with a Windows user account that has administrative privileges to log on to the system. When using incremental archiving, configure
FactoryTalk Event Archiver
to run as a Windows service with an automatic startup type. Use the
FactoryTalk Batch Service Manager
to monitor and control
FactoryTalk Event Archiver
service. See the for information on enabling
FactoryTalk Event Archiver
as a service.
To perform incremental archiving
  1. Open
    FactoryTalk® Administration Console
    and sign in to the
    FactoryTalk
    Network Directory.
  2. In
    FactoryTalk Administration Console
    Explorer
    , do one of the following:
    • For a new
      FactoryTalk Batch
      Server, right-click the application or the area name and select
      Add New Server
      FactoryTalk Batch Server
      .
    • For an existing
      FactoryTalk Batch
      Server, expand the application or the area name, right-click the server, and select
      Properties
      .
  3. In the
    FactoryTalk Batch Services Properties
    dialog, select the
    Batch Reporting
    tab.
  4. In the
    Archive method
    dropdown list, select
    Incremental Archiving
    .
  5. In the
    Archiver properties
    area, select
    Delete the event journal file after it is fully archived
    to enable the deletion of the
    .evt
    or
    .evtj
    files after
    FactoryTalk Event Archiver
    has stored the data in the ODBC database.
    IMPORTANT: Deleting files after archiving is not a reversible action and is not recommended.
  6. In
    Table name
    , type the name of the table that contains the batch data.
    The default is
    BHBatchhis
    .
  7. In
    Incremental period
    , type a value.
  8. In the
    Period units
    dropdown list, select
    Minutes
    or
    Seconds
    .
  9. To save the data in the
    Batch Reporting
    tab, select
    Apply
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal