Enable or disable archived events
The selected event types on the
Archived Events
tab identify what
electronic batch record data FactoryTalk® Event Archiver
writes to a SQL table in the
BatchHistoryEx
database.To enable or disable archived events
- OpenFactoryTalk Administration Consoleand sign in to theFactoryTalkNetwork Directory.
- InFactoryTalk Administration ConsoleExplorer, do one of the following:
- For a newFactoryTalk BatchServer, right-click the application or the area name and select .
- For an existingFactoryTalk BatchServer, expand the application or the area name, right-click the server, and selectProperties.
- In theFactoryTalk Batch Services Propertiesdialog, select theArchived Eventstab.
- To specify the event type data you want theFactoryTalk Event Archiverto collect, select or clear checkboxes next to specific event types.
- To save the data in theArchived Eventstab, selectApply.
Provide Feedback