Add a FactoryTalk Batch Server extended property

Extended properties are not available to configure in the user interface. Only configure them when directed to do so by
Rockwell Automation®
technical support.
Each property exists as a pair of strings,
Name
and
Value
.
To add a
FactoryTalk Batch
Server extended property
  1. Open
    FactoryTalk Administration Console
    and sign into the
    FactoryTalk
    Network Directory.
  2. In
    FactoryTalk Administration Console
    Explorer
    , do one of the following:
    • For a new
      FactoryTalk Batch
      Server, right-click the application or the area name and select
      Add New Server
      FactoryTalk Batch Server
      .
    • For an existing
      FactoryTalk Batch
      Server, expand the application or the area name, right-click the server, and select
      Properties
      .
  3. In the
    FactoryTalk Batch Services Properties
    dialog, select the
    Advanced
    tab.
  4. In the
    Extended properties
    area, select
    Add
    .
  5. In the
    Add Extended Property
    dialog, enter a
    Name
    and
    Value
    for the property and select
    OK
    .
  6. Select
    Apply
    to save the data in the
    Advanced
    tab.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal