Service state

The
Service State
area has buttons, text, and a graphic traffic light service state representation.
These server states and corresponding colors are shown:
Server status and their colors
Server Status
Color
STARTING
None
RUNNING
Green
STOPPED
Red
PAUSED
Yellow
NOT CONNECTED
None
START PENDING
None
The
Service State
area has these buttons:
Buttons in the Service State area
Item
Definition
Stop
Stops the selected service.
Pause
Pauses the selected service. This button is not enabled for the batch server.
Start/
Continue
Starts the selected service or continues a service that has been paused.
TIP:
The state of the
FactoryTalk Batch
Service Manager (information from the
Connection
and
Server
groups) is stored from the last time the Service Manager was run. These values are written when the
FactoryTalk Batch
Server is closed.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal