FactoryTalk Batch Server Details dialog box - View Communications tab

The
View
Communications
tab is used to monitor the number of Dynamic Data Exchange (DDE), Component Object Model (COM) and Open Platform Communications (OPC) conversations taking place between the
FactoryTalk Batch
Server and Client software.
The
View Communications
tab shows:
Items on the View Communications tab
Item
Definition
DDE Connections
The number of DDE connections attached to the
FactoryTalk Batch
Server.
COM Connections
The number of COM connections attached to the server.
OPC Connections
The number of OPC connections attached to the server.
Items
The number of connection items the server currently supports.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal