FactoryTalk Batch Server Details dialog box - PCD Communications tab

The
PCD
Communications
tab is used to monitor the
FactoryTalk Batch
Server communication status and any data servers that are communicating with the server. Verification of all tags, phases, and equipment operation sequences associated with the current area model is also performed.
The
PCD Communications
tab displays these components:
Components on the PCD Communications tab
Field
Definition
Data Server Status
Lists of all configured data servers in the area model and the communication status between
FactoryTalk Batch
and these data server(s).
Tag Verify Status
Indicates if the verification function is READY, IN PROGRESS, or COMPLETED.
Tag Verify Verified
Indicates the number of tags, phases, and equipment operation sequences that the server processed during tag verification.
Tag Verify Bad
Indicates the number of tags, phases, and equipment operation sequences that the server was unable to verify. Bad tags, phases, and equipment operation sequences indicate either the data server cannot supply the data requested by the
FactoryTalk Batch
Server or the data was not of the expected type.
Tag Verify Total
Indicates the total number of tags, phases, and equipment operation sequences.
Start
Starts the verification process.
Stop
Stops the verification process.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal