FactoryTalk Batch Server Details dialog box - Messages tab

The
Messages
tab is used to monitor
FactoryTalk Batch
Server log information. The messages displayed in the three sections are the most recent messages written to the server log by the server.
The
Messages
tab shows:
Items on the Messages tab
Field
Definition
Info
The most recent
Info
-type entry in the log file.
Info
entries are log entries recorded as a part of the normal execution.
Warning
The most recent
Warning
-type entry in the log file.
Warning
entries indicate that a minor irregularity the system detected. The irregularity was handled by the system or the system is not sure of the occurrence’s implications.
Severe
The most recent
Severe
-type entry in the log file.
Severe
entries indicate that the system encountered a severe error condition. The system handled the situation as best it could.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal