FactoryTalk Batch Server Details dialog box - General tab

The
General
tab lists data on the number of batches and prompts being currently handled by the
FactoryTalk Batch
Server, as well as the Windows time on the server, the time the batch server started, and the name and creation date of the current area model.
The
General
tab shows:
Items on the General tab
Field
Definition
Batch Count
The number of batches loaded in the
FactoryTalk Batch
Server.
Prompts Count
The number of prompts currently existing within all batches.
Version
The version number of the
FactoryTalk Batch
Server.
Time
The time as specified by Windows on the
FactoryTalk Batch
Server.
Started at
The time the
FactoryTalk Batch
Server started.
Area Model File Name
The name of the currently active area model.
Area Model Date
The file date of the currently active area model at the time of
FactoryTalk Batch
Server startup or the last update.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal