Cross invocation string escape sequences

The escape sequences used in the cross invocation strings correspond to the current selection the in the
FactoryTalk Batch View HMI Controls
. The context data passed to the automation server is relative to the current selection.
The table describes each escape sequence relative to the type of procedural element selected:
Escape sequence descriptions
Escape Sequence
Procedure
Unit Procedure
Operation
Phase
%P
Path
Path
Path
Path
%N
Corresponding Process Cell Name
Corresponding Unit name
Corresponding Unit name
Corresponding Phase name
%C
Corresponding Process Cell class name
Corresponding Unit Class name
Corresponding Unit Class name
Corresponding Phase Class name
%T
1 (Process Cell)
2 (Unit)
2 (Unit)
3 (Phase)
%S
Node
Node
Node
Node
%B
Batch ID
Batch ID
Batch ID
Batch ID
%M
Menu caption
Menu caption
Menu caption
Menu caption
%R
Corresponding Process Cell resource ID
Corresponding Unit resource ID
Corresponding Unit resource ID
Corresponding Phase resource ID
If the control recipe runs across multiple process cells, the context data replaced by %N and %C is the first process cell in the process cells list of associated with the recipe.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal