Add users and user groups

Set security on folders and files to limit log file and event journal (.evt or .evtj) access.
To add users and user groups:
  1. In
    Windows Explorer
    , locate the folder or file.
  2. Right-click the folder or file, and then select
    Properties
    .
  3. Select the
    Security
    tab, select
    Edit
    , and then select
    Add
    .
  4. From the
    Select Users
    ,
    Computers, Service Accounts, or Groups
    dialog box, select
    Advanced
    and then click
    Find Now
    .
  5. Select a user or group from the
    Search results
    list, and then select
    OK
    .
  6. Repeat for each user or group that requires access to the folder or file.
    TIP:
    Be sure to add the
    FactoryTalk Batch
    Server user account and then configure the account with
    Full Control
    permissions.
  7. Select
    OK
    to return to the
    Properties
    dialog box.
  8. From the
    Group or user name
    list, select a user or group, and then select the permissions in the
    Permissions
    area. Repeat for each user or group.
  9. Select
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal