Add the Batch COM service

To add the COM service, run the
BatchIDCreationCOMPlusInstall
script and then add the server user account to the
FactoryTalk Batch
Server service,
FactoryTalk Event Archiver
service, and the Batch COM+ Application. If
FactoryTalk
e
Procedure
is part of your system, add the server user account to the
e
Procedure
Server service.
To add the Batch COM service:
  1. In Windows Explorer, expand
    Program Files x86 > Rockwell Software > Batch > Scripts
    .
  2. Double-click
    BatchIDCreationCOMPlusInstall.vbs
    to add the
    FactoryTalk Batch
    COM service to the computer.
  3. Select
    Start > Windows Administrative Tools > Component Services > Computers > My Computer > COM+ Applications
    .
  4. Right-click
    Batch > Properties
    .
  5. Select the
    Identity
    tab, select
    This user
    , and enter the user name and password for the
    FactoryTalk Batch
    Server.
  6. Select
    OK
    and then close Component Services.
  7. Select
    Start > Windows Administrative Tools > Services
    .
  8. Right-click
    FactoryTalk Batch Server > Properties
    .
  9. Select the
    Log On
    tab and then select
    This Account
    .
  10. Enter the user account name and password for the server.
  11. Select
    OK
    .
    • Add the server user account to FactoryTalk Event Archiver service if you are using FactoryTalk Event Archiver in incremental mode.
    • Add the server user account to the
      e
      Procedure
      Server service if
      e
      Procedure
      is part of your
      FactoryTalk Batch
      system.
  12. Close
    Services
    .
  13. Restart the computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal