FactoryTalk Batch Server install configuration
The installation of the FactoryTalk Batch Server creates the Windows user group
FTBatchServiceAccounts
on the FactoryTalk Batch Server. This group
is automatically assigned all the user rights and default access permissions required for
the FactoryTalk Batch Server to function correctly.The installation adds the FactoryTalk Batch Server user account to the following:
- FTBatchServiceAccounts
- MasterRecipeViewer
- Batch COM+ Application
- FactoryTalk Batch Server service
- FactoryTalk Event Archiver service
- FactoryTalkeProcedure Server service (eProcedure Server installation)
The services for the FactoryTalk Batch Server, FactoryTalk Event Archiver, FactoryTalk
e
Procedure Server, and the Batch COM+ Application require identical user accounts
to support the FactoryTalk Batch Server functionality.Provide Feedback