FactoryTalk Security for the Batch Clients

Security settings are shared among
FactoryTalk
enabled products across a network or on the same computer using
FactoryTalk® Security
in
FactoryTalk® Batch View
,
FactoryTalk® Batch View HMI Controls
,
FactoryTalk Batch Equipment Editor
, and
FactoryTalk Batch Recipe Editor
.
FactoryTalk® Directory
is the infrastructure which contains the policies defined for products and resources.
FactoryTalk Batch
product policies are created in both the Local Directory and the Network Directory when the
FactoryTalk® Services Platform
is installed. The
FactoryTalk Batch
product polices are used to restrict access to the
FactoryTalk Batch
Client components and their features. For a complete list of
FactoryTalk Batch
secured resources and their default product policy settings, see
FactoryTalk Batch
default policy settings.
The following information is specific to configuring
FactoryTalk
Security for the
FactoryTalk Batch
Clients. For information on securing your
FactoryTalk
system as a whole, see
FactoryTalk Help
.
To open
FactoryTalk
Help, click
Start > Rockwell Software > FactoryTalk Help
.
The
FactoryTalk Services Platform
installation process:
  • Creates a FactoryTalk Local Directory and a FactoryTalk Network Directory on the computer.
    When the install process finishes, both directories are fully configured and ready for use.
    TIP:
    Security settings in the Network Directory are completely separate from the security settings in the Local Directory. For example, changes made to the security settings in the Network Directory do not change security settings in the Local Directory.
  • Allows any Windows Administrator user account to log on to either directory.
    The installation process automatically adds the local Windows Administrators group to the
    FactoryTalk
    Administrators group in each
    FactoryTalk Directory
    .
  • Allows any authenticated Windows user to log on to the FactoryTalk Local Directory.
    The installation process automatically adds all members of the local Windows Authenticated Users group to the
    FactoryTalk
    Local Directory.
  • Allows all new user accounts full access permissions.
    The installation process automatically sets system policies to allow all new user accounts added to either directory full access to that directory by default.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal