Unit Bind Signature request

Overview

If a Bind Command Verification policy is configured in the area model and it is associated with a Signature Template, then a
Unit Bind Signature
request is generated when a user attempts to bind a Unit to a step.

Modifications made to support FactoryTalk Batch electronic signatures

The following is an explanation of the modifications made to support
FactoryTalk® Batch
electronic signature:
Modifications made to support FactoryTalk Batch electronic signatures
Bind Execute
Batch Server
When the
FactoryTalk Batch
Server receives a legal Bind execute, the Area Model configuration is checked to determine if a confirmation signature is required for the Bind request. If one is required, then a Signature Request is generated using the specified Signature Template and the Bind action is queued pending Signature completion.
Response
An ActionID is returned by the Execute used to locate the generated signature.
Completion
When all Signature Signoffs associated with a Bind Execute Action are completed, then the Unit Requirement targeted by the Bind Execute Action is bound to the specified Unit if the bind action is still legal.
Cancellation
When any Signature generated by a Bind Execute Action is cancelled, then the Bind Action is terminated and its associated incomplete Signature Requests are System Cancelled.
Overlap
If a Bind Execute is received while an earlier Bind Execute Action is pending for the same target Unit Requirement, then the new Bind Execute fails. The failed execute’s response item is populated with an appropriate response string. For purposes of determining the legality of overlapping executes, Command, Step, Remove, and BindPhase Executes are treated as being Bind Executes. This means, for example, that if a Step Execute Action is pending Signature completion on a procedure, then a Bind Execute to the same procedure fails because of the overlap with the Step execute.
Automatic Cancellation
If any step associated with the Unit Requirement being targeted by a queued Bind Execute Action becomes an active recipe element, then the Bind Execute Action is terminated and its associated incomplete Signature Requests are System Cancelled. This happens because the Bind action is not legal for a Unit Requirement associated with any active steps.
Warm Restart, Warm All Restart, or Hot Restart
Signature Requests generated in response to a Bind Execute Action are restored in the event of a
FactoryTalk Batch
Server Warm Restart, Warm All Restart, or Hot Restart.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal