Unit Bind Prompt Acknowledge Signature request

Overview

If a Bind Ack Command Verification policy is configured in the area model and it is associated with a Signature Template, then a
Unit Bind Prompt Acknowledge Signature
request is generated when binding a Unit to a step after a prompt has been generated or prompting binds a Unit to a step.

Modifications made to support FactoryTalk Batch electronic signatures

The following is an explanation of the modifications made to support
FactoryTalk® Batch
electronic signatures:
Unit Bind Execute
Unit Bind Execute
Batch Server
When the
FactoryTalk Batch
Server receives a legal Ack execute in response to a Unit Bind UnacknowledgedEvent, it may queue the bind selection delivery pending a Signature Request if such behavior is configured in the area model.
Response
An ActionID is returned by the Execute used to locate the generated signature.
Completion
When all Signature Signoffs generated by an Ack received in response to a Unit Bind UnacknowledgedEvent are completed, then the Unit Requirement binds to the Ack execute response Unit specified if the bind action is still legal.
Cancellation
When any Signature generated by a Unit Bind Ack execute is cancelled, then the Unit Bind Ack Action is terminated and its associated incomplete Signature Requests are System Cancelled.
Overlap
If a Unit Bind Ack execute response to a Unit Bind Prompt is received while there are existing incomplete Signature Requests generated by a prior Unit Bind Ack Action targeting the same prompt, or the Batch has a Remove Action pending, then the new execute fails. The failed execute’s response item is populated with an appropriate error message string.
Automatic Cancellation
If the batch system cancels an UnacknowledgedEvent targeted by a Unit Bind Ack Action, then the queued Execute Action is terminated and all incomplete Signature Requests associated with the Action are System Cancelled.
Warm Restart, Warm All Restart, or Hot Restart
Signature Requests generated in response to a Unit Bind Ack Execute Action are System Cancelled in the event of a
FactoryTalk Batch
Server Warm Restart, Warm All Restart, or Hot Restart.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal