Remove Batch Signature request

Overview

If a Remove/Reset Command Verification policy is configured in the area model and it is associated with a Signature Template, then a
Remove Batch Signature
Request is generated when a user attempts to remove a batch from the Batch List or reset a phase run under Manual Phase Control.

Modifications made to support FactoryTalk Batch electronic signatures

The following is an explanation of the modifications made to support
FactoryTalk® Batch
electronic signatures:
Modifications made to support FactoryTalk Batch electronic signatures
Remove Execute
Batch Server
When the
FactoryTalk Batch
Server receives a legal Remove execute, the area model configuration is checked to decide if a confirmation Signature is required for the batch removal request. If one is required, then a Signature Request is generated using the specified Signature Template and the batch removal action is queued pending completion of the Signature Request.
Manual Phase Control - When the server receives a legal Phase Reset Execute, it checks the area model configuration to decide if a confirmation signature is required. If so, then a Signature Request is generated using the specified Signature Template and the phase reset action is queued pending the Signature Request completion.
Response
An ActionID is returned by the Execute used to locate the generated signature.
Completion
When all Signature Signoffs associated with a Remove Execute are completed, then the batch specified in the Remove execute is removed from the batch list if the Remove instruction is still legal.
When all Signatures associated with a Phase Reset are complete, then the Manual Phase Control batch specified in the Phase Reset Execute is removed from the Batch List if the Phase Reset instruction is still legal.
Overlap
If a Remove Execute is received targeting a batch for which a queued Remove Execution Action already exists pending Signature completion(s), then the new Remove Execute fails. The failed execute’s response item is populated with an appropriate response string.
If a Phase Reset Execute is received targeting a batch for which a queued Phase Reset Execution Action already exists pending Signature completion(s), then the new Phase Reset Execute fails.
For purposes of determining the legality of overlapping of executes, Remove Executes are treated as Phase Reset Executes. This means that if a Remove Execute action is pending Signature completion on a Manual Phase Control batch, then a Phase Reset issued via a Phase Execute to the same batch fails because of the Remove Execute overlap.
Cancellation
When an incomplete Signature associated with a Remove Execute Action is cancelled, then the queued Remove Execute Action is terminated and its associated incomplete Signature Requests are System Cancelled.
When an incomplete Signature associated with a Phase Reset Execute Action is cancelled, then the queued Phase Reset Execute Action is terminated and its associated incomplete Signature Requests are System Cancelled.
Automatic Cancellation
A Remove Execute Action that is queued pending Signature Completion(s) is terminated if the target batch changes to an illegal state for Batch Removal, resulting in System Cancellation of its incomplete Signature Request(s).
A Phase Reset Execute Action that is queued pending Signature Completion(s) is terminated if the target batch changes to an illegal state for Batch Removal, resulting in System Cancellation of its incomplete Signature Request(s).
Warm Restart, Warm All Restart, or Hot Restart
Signature Requests generated in response to a Phase Reset or a Remove Execute Action are System Cancelled in the event of a
FactoryTalk Batch
Server Warm Restart, Warm All Restart, or Hot Restart.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal