Phase Bind Prompt Acknowledge Signature request
Overview
If a Bind Ack Command Verification policy is configured in the area model and it is
associated with a Signature Template, then a
Phase Bind
Signature
request is generated when binding a phase to a material
after a prompt is generated or prompting binds a phase to a material.Modifications made to support FactoryTalk Batch electronic signatures
The following is an explanation of the modifications made to support
FactoryTalk® Batch
electronic signatures:Recipe Phase Bind Ack Execute | |
|---|---|
Batch Server | When the FactoryTalk Batch Server receives a legal Ack
execute in response to a Recipe Phase Bind UnacknowledgedEvent,
it may queue the bind selection delivery pending a Signature
Request if such behavior is configured in the area model. |
Response | An ActionID is returned by the Execute used to locate the
generated signature. |
Completion | When all Signature Signoffs generated by an Ack received in
response to a Recipe Phase Bind UnacknowledgedEvent are
completed, then the Recipe Phase is bound using the Ack execute
response data specified if the bind action is still legal. |
Cancellation | When any Signature generated by a Recipe Phase Bind Ack Execute
is cancelled, then the Recipe Phase Bind Ack Action is
terminated and its associated incomplete Signature Requests are
System Cancelled. |
Overlap | If an Ack execute response to a recipe Phase Bind Prompt is
received while there are existing incomplete Signature Requests
generated by a prior Ack to the same prompt, or the Batch has a
Remove Action pending, then the new execute fails. The failed
execute’s response item is populated with an appropriate error
message string. |
Automatic Cancellation | If the batch system cancels an UnacknowledgedEvent targeted by a
Recipe Phase Bind Ack Action, then the queued Execute Action is
terminated and all incomplete Signature Requests associated with
the Action are System Cancelled. |
Warm Restart, Warm All Restart, or Hot Restart | Signature Requests generated in response to a Recipe Phase Bind
Ack Execute Action are System Cancelled in the event of a FactoryTalk Batch Server Warm Restart, Warm All Restart, or Hot Restart. |
Provide Feedback