Active Step Change Signature request

Overview

If a Step Command Verification policy is configured in the area model and associated with a signature template, then an
Active Step Change Signature
request is generated when performing an active step change.

Modifications made to support FactoryTalk Batch electronic signatures

The following is an explanation of the modifications made to support
FactoryTalk® Batch
electronic signatures:
Modifications made to support FactoryTalk Batch electronic signatures
Step Execute
Batch Server
When the
FactoryTalk Batch
Server receives a legal Step execute, the Area Model configuration is checked to decide if a confirmation signature is required for the Active Step Change action. If one is required, then a signature request is generated using the specified signature template and the Active Step Change action is queued pending signature request completion.
Response
An ActionID is returned by the execute used to locate the generated signature.
Completion
When all signatures associated with a Step execute action are completed, then the queued Step execute action is performed if it is still legal.
Cancellation
When any signature generated by a Step execute action is cancelled, then the Active Step Change action is terminated and its associated incomplete Signature Requests are System Cancelled.
Overlap
When a Step execute is received targeting a procedure that already has a pending Step execute action, then the new Step execute fails. The failed execute’s response item is populated with an appropriate error message.
For purposes of determining overlapping legality executes, the Command and Remove execute actions are treated as being Step execute actions. This means, for example, that if a Step execute action is pending signature completion, then an AUTO command issued via a Command execute to the same procedure fails because of the overlap with the Step execute action.
Warm Restart, Warm All Restart, or Hot Restart
Signature requests generated in response to a Step execute action are cancelled in the event of a
FactoryTalk Batch
Server Warm Restart, Warm All Restart, or Hot Restart.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal