Electronic signature security
FactoryTalk
Security is used to support FactoryTalk Batch
Electronic Signature Signoffs. The ESignature Network Directory
policy setting is
created in the FactoryTalk
Local Directory during FactoryTalk Batch
installation with a default value of True
. The value of the ESignature Network
Directory
policy setting determines whether the users and groups defined in the FactoryTalk
Local Directory or the users and groups defined in the FactoryTalk
Network Directory are used to assign Security Permissions to Electronic Signature
Templates and validate Electronic Signature Request Signoffs. Security Permissions for Signature Signoffs are specified when the Signature Template is
created in
FactoryTalk Batch Equipment Editor
. The Security Permissions defined in the Signature Template are required to complete the
Signoff(s) generated in the associated Signature Request. Each Signoff requires a UserID and
a password. When a signature requires multiple signoffs, each signoff must be made using a
unique UserID and password.Signature templates are also used for Recipe Approval process signoffs, and must be configured before recipe approvals can be enabled, configured, and executed.
For more information on configuring signature templates, see the .
Provide Feedback