Audited FactoryTalk Batch Recipe Editor events
This section describes audit messages that
FactoryTalk Batch Recipe Editor
generates in
response to recipe modifications and operations.Message Type | Event |
|---|---|
Recipe Object | Open an existing recipe Create a new recipe Save a recipe, including master recipes and recipe formulations Save all recipes, including master recipes and recipe formulations Remove a recipe (User-supplied comment when deleting) Import a recipe (User-supplied comment when importing) Export a recipe (User-supplied comment when exporting) Rebuild the recipe directory (User-supplied comment when rebuilding recipe) Delete an existing recipe, including master recipes and recipe formulations Update an existing recipe, including master recipes and recipe formulations |
Recipe Print | Print a procedure, unit procedure, or operation |
Recipe Header | Edit or update recipe header properties, except the recipe name |
Recipe Step | Add a recipe step, insert step, or parallel recipe step Edit or update a recipe step Delete a recipe step |
Recipe Approval Step | Sign off on an approval step Revert an approval step |
Recipe Versioning | Check in a recipe (create a new version of a recipe) Check out a recipe [create a work-in-progress (WIP) recipe] Obsolete a recipe Save an obsolete recipe Reinstate an obsolete recipe Save a reinstated recipe Version conflict on recipe import Version conflict on recipe directory rebuild, including auto rebuild of the
directory when FactoryTalk Batch Recipe Editor opensDelete a recipe due to version conflict resolution during import or recipe directory rebuild Remove sign-off(s) due to verification failure for versioned and non-versioned
recipes |
Recipe Security | Change a recipe security state Edit or change a security authority identifier (SAI) Change a FactoryTalk® Services Platform SAI host
computer |
Recipe Text Box | Add a text box Delete a text box Edit a text box (only if the comment changes) Associate a text box Disassociate a text box |
Recipe Formula Parameter | Add a recipe formula parameter to a step Delete a recipe formula parameter from a step Edit or update a recipe formula parameter of a step |
Recipe Formulation | Add a recipe formulation Delete a recipe formulation Duplicate a recipe formulation Rename a recipe formulation Change the recipe formulation description |
Recipe Formulation Parameter | Edit or update a recipe formulation parameter |
Formula Value | Edit or update a formula value’s non-origin properties Edit or update a formula value’s origin property Edit or update a formula value’s value property for deferred parameters |
Report Limit | Add a report limit Delete a report limit Edit or update a report limit |
Bind Requirement | Add or update a bind requirement Delete a bind requirement |
Bind Preference | Add or update bind preference Delete a bind preference |
Recipe Transition | Add a transition to a recipe Edit or update a recipe transition Delete a transition to a recipe |
Link Group | Add a recipe link group Delete a recipe link group Edit or update a recipe link group |
Equipment Requirement | Add an equipment requirement to a recipe Delete an equipment requirement of a recipe Edit or update procedure-only equipment requirement properties, except downstream
units Edit or update procedure-only equipment requirement’s downstream units
property Edit or update operation and unit procedure equipment requirements |
Recipe Verification | Verify a single recipe Verify all recipes |
Material Loop | Add a material loop to a recipe Undo a material loop |
Recipe Link | Add a recipe link Delete a recipe link |
Provide Feedback