Audited FactoryTalk Batch Equipment Editor events
This section describes the set of audit messages generated by
FactoryTalk Batch Equipment Editor
. Not all user actions are audited; for example, View
menu changes and
Options
menu changes do not generate audit messages. The following events are
audited when the area model is saved.Message Type | Event |
|---|---|
Area Model | Invoke FactoryTalk Batch Equipment Editor Open an existing area model Create a new area model Save an area model Edit/update an area model property Delete an area model Add a signature template Delete a signature template Update a signature template Enable/disable recipe approvals Enable/disable recipe versioning Update a command verification policy |
Area Model Security | Security authority is configured for an area model Security authority identifier (SAI) is set or removed Security authority configuration change is accepted by user Security authority changes are saved to the area model |
Data Server | Add an OPC® serverDelete an OPC server Edit/update an OPC server property Add a Logix5000™
CIP™ serverDelete a Logix5000 CIP server Edit a Logix5000 CIP server Add an FTD server Delete an FTD server Edit/update an FTD server property |
Enumeration Set | Create an enumeration set Delete an enumeration set Edit/update an enumeration set property |
Enumeration | Add an enumeration Delete an enumeration Edit/update an enumeration property |
Resource Class | Add a resource class Delete a resource class Edit/update a resource class property |
Resource | Add a resource Delete a resource Edit/update a resource property |
Process Cell Class | Add a process cell class Copy a process cell class Delete a process cell class Edit/update a process cell class property |
Process Cell | Add a process cell Copy a process cell Delete a process cell Edit/update a process cell property |
Unit Attribute | Add a unit attribute Delete a unit attribute Edit/update a unit attribute property |
Unit | Add a unit Copy a unit Edit a unit Delete a unit Edit/update a unit property |
Global Unit Binding Requirements | Add global unit attribute Edit global unit attribute Delete global unit attribute |
Unit Flow Path | Link units with a flow path Unlink units with a flow path |
Equipment Phase Class (Recipe Phase) | Add an equipment phase class Copy an equipment phase class Delete an equipment phase class Edit/update an equipment phase class property Edit/update an equipment phase class control strategy set of parameters Edit/update an equipment phase class optional material parameters property Edit/update an equipment phase class control strategy set of reports Edit/update an equipment phase class control strategy |
Equipment Phase | Add an equipment phase Copy an equipment phase Delete an equipment phase Edit/update an equipment phase property Edit/update an equipment phase’s server property Reset an equipment phase’s tags to default values Share an equipment phase between units |
Recipe Parameter | Add a recipe parameter Delete a recipe parameter Edit/update a recipe parameter property |
Recipe Approval Step | Add a recipe approval step Delete a recipe approval step Edit/update a recipe approval step |
Report Parameter | Add a report parameter Delete a recipe parameter Edit/update a recipe parameter property |
Phase Message | Add a phase message Delete a phase message Edit/update a phase message property |
Synchronize | Synchronize a phase |
Tag Class | Add a tag class Delete a tag class Edit/update a tag class property |
Unit Attribute Tag | Add a unit attribute tag Delete a unit attribute tag Edit/update a unit attribute tag property |
Container Association | Add a container association Delete a container association Edit/update a container association property |
Instruction Configuration | Edit/update an instruction configuration property |
Phase Tag | Edit/update a phase tag property |
Provide Feedback