View audit messages in the FactoryTalk AssetCentre client

View the audit messages through the
FactoryTalk
AssetCentre client.
To view the audit messages in the FactoryTalk AssetCentre client:
  1. To open the
    FactoryTalk
    AssetCentre client,
    Start
    button, point to
    All Programs > Rockwell Software > FactoryTalk AssetCentre
    , and then click
    FactoryTalk
    AssetCentre.
  2. Click the
    Logs
    button to open the Logs view.
    TIP:
    For information about using or customizing the
    FactoryTalk
    AssetCentre client, refer to the utility's online help or the
    FactoryTalk AssetCentre Installation Guide
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal