Windows event log entries

FactoryTalk Event Archiver
creates Windows event log entries during startup, run time, and shutdown.
FTB_Admin_EventLog
Log entries contain:
Log entries
Name
Description
Date
Date that the event occurred
Time
Time that the event occurred
Type
Type of event, such as
Information
or
Error
User
Configured domain user
Computer
Computer on which
FactoryTalk Event Archiver
runs
Source
BATCHARC.log
file
Category
Category of the event
Event ID
ID of the event
Description
Description of the event
Data
File name and line number from the
FactoryTalk Event Archiver
source code that generated the entry
These
FactoryTalk Event Archiver
events can occur and be entered in the Windows event log:
FactoryTalk Archiver events that can occur and be entered in the Windows event log
Category
Event
Description
Start
1001
FactoryTalk Event Archiver
Service started successfully in incremental mode
Start
1002
FactoryTalk Event Archiver
Process started successfully in non-incremental mode
Start
1003
FactoryTalk Event Archiver
failed to start; see the
BATCHARC.LOG
file for more information
Start
1004
FactoryTalk Event Archiver
failed to open the
BATCHARC.LOG
file
Start
1005
Service handler not installed
Start
1006
Bad Service Request
Start
3001
FactoryTalk Event Archiver
Service paused
Start
3002
FactoryTalk Event Archiver
Service continuing
Shutdown
4001
FactoryTalk Event Archiver
Service shutting down
Setup
5001
FactoryTalk Event Archiver
setup; new connect string = <new string>
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal