Forward/Backward Track and Trace Report

Material Manager
automatically creates these parameters:
Parameters created by FactoryTalk Batch Material Manager
Parameter
Description
Formula Parameter:
lot
Report Parameter:
actual_amount
Without
Material Manager
, define these Formula and Report parameter names:
Formula and Report parameter names to be defined without FactoryTalk Batch Material Manager
Parameter
Description
Report Parameter:
lot_xx_yy (where xx is user defined and yy represents an incremental lot #)
Report Parameter:
actual_lot_xx_yy (where xx is user defined and yy [optional] represents an incremental lot )
Single lot with single actual. Without yy value.
Add phase example:
Add phase example
Parameter
Description
Report Parameter:
lot_oil
Report Parameter:
actual_lot_oil
Single lot with single actual. With yy value.
Add phase example:
Add phase example
Parameter
Description
Report Parameter:
lot_oil_01
Report Parameter:
actual_lot_oil_01
Multiple lots with multiple actuals.
Add phase example:
Add phase example
Parameter
Description
Report Parameter:
lot_oil_01
Report Parameter:
lot_oil_02
Report Parameter:
actual_lot_oil_01
Report Parameter:
actual_lot_oil_02
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal