Single Specific Ingredient Addition Phase with target_xx parameter
This is an example of Single Specific Ingredient Addition Phase with target_xx parameter:
Parameter | Description |
|---|---|
Formula Parameter: | Material_Oil |
Formula Parameter: | Setpoint_Oil |
Report Parameter: | Lot_Oil |
Report Parameter: | Actual_Lot_Oil |
Report Parameter: | Target_Oil |
Report Parameter: | Actual_Oil |
Report Parameter: | In_Tolerance_Oil |
Provide Feedback