Multiple Specific Ingredient Addition Phase
This is an example of Multiple Specific Ingredient Addition Phase:
Parameter | Description |
|---|---|
Formula Parameter: | Material_Oil |
Formula Parameter: | Material_HFCS |
Formula Parameter: | Setpoint_Oil |
Formula Parameter: | Setpoint_HFCS |
Report Parameter: | Lot_Oil |
Report Parameter: | Lot_HFCS |
Report Parameter: | Actual_Lot_Oil |
Report Parameter: | Actual_Lot_HFCS |
Report Parameter: | Target_Oil |
Report Parameter: | Target_HFCS |
Report Parameter: | Actual_Oil |
Report Parameter: | Actual_HFCS |
Report Parameter: | In_Tolerance_Oil |
Report Parameter: | In_Tolerance_HFCS |
Provide Feedback