Material usage

These tables outline the different components of the report.
Datasets
Datasets
Dataset
Stored Procedure
Comment
GetMaterialID
spGetMaterialIDByDate
Gets the Material IDs used between two dates
GetMaterialUsageData
spGetMaterialUsageData- ByDate
Gets the Material amounts used between two dates
GetRecipeNames
spGetRecipeNamesBYDate
Gets the Recipes used between two dates
GetUnitName
spGetUnitNameByDate
Gets the Units used between two dates
GetProcessCell
spGetProcessCellByDate
Gets the Process Cells used between two dates
GetAreaNames
spGetAreaNamesByDate
Get Area Names between two dates
Report Parameters
Report Parameters
Parameter
Where used
Comment
StartTime
All Procedures
Start Time
EndTime
All Procedures
End Time
SearchWord
NA
User Defined Batch Filter
ProcessCell
NA
Process Cell Filter
RecipeName
NA
Recipe Name Filter
UnitName
NA
Unit Name Filter
MaterialName
GetMaterialUsageData
Material Parameter
AreaName
All Procedures
Area Name
Heading Data
Heading Data
Object
Data Item
Data Source
Type
Start Time
StartTime
User input
Parameter
End Time
EndTime
User input
Parameter
Material Name
materialname
GetmaterialUsageData
Data
Total Consumed
TotalUsed
GetmaterialUsageData
Data
Table Datasets
Table Datasets
Table
Dataset
Comment
table1_ GetmaterialUsageData
GetmaterialUsage- Data
Material Usage
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal