Batch exceptions

The following tables outline the different components of the report.
Datasets
Datasets
Dataset
Stored Procedure
Comment
GetUniqueID
spGetUniqueIDByDate
Gets the unique IDs used between two dates
GetRecipeNames
spGetRecipeNamesBYDate
Gets the recipes used between two dates
GetUnitName
spGetUnitNameByDate
Gets the units used between two dates
GetProcessCell
spGetProcessCellByDate
Gets the process cells used between two dates
AbnormalState- Changes
Embedded Query
Get the abnormal state changes for a unique ID
GetUniqueID_ BatchIDForAlarms
Embedded Query
Gets alarms
GetIntoleranceData
Embedded Query
Gets In tolerance data
GetBatchFailures
Embedded Query
Gets batch failures
GetAreaNames
spGetAreaNamesByDate
Get Area Names between two dates
Report Parameters
Report Parameters
Parameter
Where used
Comment
StartTime
All Procedures
Start Time; can be set to Null
EndTime
All Procedures
End Time; can be set to Null
SearchWord
NA
User Defined Batch filter
ProcessCell
NA
Process Cell filter
RecipeName
NA
Recipe Name filter
UnitName
NA
Unit Name filter
UniqueID
NA
Unique ID filter
AreaName
All Procedures
Area Name
Heading Data
Heading Data
Object
Data Item
Data Source
Type
Start Time
StartTime
User input
Parameter
End Time
EndTime
User input
Parameter
Table Datasets
Table Datasets
Table
Dataset
Comment
table1_AbnormalState- Changes
AbnormalState- Changes
Abnormal State Changes
table_Alarms
GetUniqueID_BatchIDForAlarms
Alarms
table_BatchFailures
GetBatchFailures
Batch Failures
table_OutOfTolerance
GetIntoleranceData
Out of Tolerance data
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal