Output table

This table describes the schema of the BHBATCHHIS table in the BatchHistoryEx database. Use this schema as the basis for developing a custom output table.
TIP:
SQL Server
columns that have a box type of
ntext
only retrieve 256 characters at a time using a standard SELECT statement. To retrieve all the data, use the READTEXT function.
Schema of the BHBATCHHIS table in the BatchHistoryEx database
Name
Type
Description
Example
GMT
datetime NULL
Time event is recorded in Greenwich Mean Time
2003-04-29 12:21:01.000
lclTime
datetime NULL
Local time of event
2003-04-29 14:52:07.000
UniqueID
varchar(12) NULL
Unique identifier assigned by the
FactoryTalk Batch
Server
31
BatchID
varchar(255) NULL
Alpha Batch ID
BATCH_ID-030102-3
Recipe
varchar(1000) NULL
The recipe element that was executing at the time of the electronic batch record entry. The box contents appear as:
<UniqueID>:[<Procedure>\][<Unit Procedure>:Instance\] <Operation>:Instance-LoopCounter
The data in the brackets is optional, depending on the recipe level.
13:Y_300_YELLOW_PAINT
Descript
varchar(255) NULL
Description of PValue data
Yellow Paint
Event
varchar(155) NULL
Event type triggering the record
Material Tracking / Material Bound / Material Unbound
PValue
varchar(255) NULL
Value reported to the electronic batch record
50
DescriptAPI
varchar(255) NULL
Description of PValue data
Engineering Units
EventAPI
varchar(155) NULL
Event type triggering the record
Report
PValueAPI
varchar(255) NULL
Value reported to the electronic batch record
50
EU
varchar(255) NULL
Engineering units associated with PValue
GALLONS
Area
varchar(155) NULL
Area model name in batch equipment configuration where batch was executed
THE_PAINT_COMPANY
ProcCell
varchar(155) NULL
Process cell in batch equipment configuration
YELLOWPAINT1
Unit
varchar(155) NULL
Unit name in batch equipment configuration
PREMIX_A
Phase
varchar(155) NULL
Name of the phase generating the record
PROC_ORDER_N
Printed
datetime NULL
Last date the batch report was printed
2003-04-29 14:52:07.000
UserID
varchar(85) NULL
Computer name/Windows user name
mjames1
PhaseDesc
varchar(50) NULL
Phase class description
MaterialName
varchar(155) NULL
Common name of the material
YELLOWPAINT
MaterialID
varchar(50) NULL
Inventory control system material ID used to track the material
31
LotName
varchar(255) NULL
Name assigned to a lot of material
TEST317_BRAND
Label
varchar(255) NULL
ID assigned to a distributed portion of a lot
STANDARDBRANDYELLOW
Container
varchar(255) NULL
Container’s name where material and lot were distributed, or where material and lot are stored
WAREHOUSE2/PAINT_PALLET1
PromiseID
varchar(50) NULL
Unique ID used as a key to allow grouping of separate event entries all resulting from a single material addition
100
Signature
varchar(255) NULL
Used for event journal signatures by Batchsig program to detect changes in
.evt
file. Information stored here is a hexadecimal or a single spaced character.
ERP_Flag
varchar(1) NULL
Tag indicating information reported to SAP
RecordNo
int NULL
Unique identifier assigned to the record when it is added to the database
31
ArchivedGMT
datetime NULL
Date and time
2003-04-29 14:52:07:000
Reactivation Number
int
Number of times an active
e
Procedure
control step has been reactivated
1
InstructionHTML
ntext
HTML for completed
e
Procedure
instruction steps
<FORM>
Add a CIP batch to the Batch List. Select
OK
when done.
</FORM>
SignatureID
int
A 32-bit unsigned integer that uniquely identifies a Signature Request within the batch system.
1
ActionID
int
A 32-bit unsigned integer that uniquely identifies an Action within the batch system. An Action is a queued Execute command to the
FactoryTalk Batch
Server that is pending one or more Signature completions prior to execution.
1
ContextsID
varchar(255) NULL
Supports Context ID reporting. Lists the ContextID enumeration set member ordinals assigned to the input or output parameter for event generation.
Contexts
varchar(1024) NULL
Supports Context ID reporting. Lists the ContextID enumeration set member strings assigned to the input or output parameter for event generation.
RecordID
PK, varchar(255) NOT NULL
The primary key.
IDEVSE110010Sep 3 2014881157
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal