Run FactoryTalk Event Archiver

When using End of Batch Archiving, the
FactoryTalk Batch
Server runs
FactoryTalk Event Archiver
after a batch is removed from the batch list. When using Incremental Archiving,
FactoryTalk Event Archiver
runs continuously during batch execution and archives batch data at user-defined time increments. The
FactoryTalk Batch
Service Manager controls the Archiver Service.
The Batch Service Manager must communicate with the Windows Service Manager of the selected computer to determine available services. A noticeable delay may exist while communications are established. If the Batch Service Manager cannot communicate with the Windows Services, an error message is displayed.
Before you begin:
The user who is running the
FactoryTalk Batch Service Manager
must have administrative privileges on the computer where
FactoryTalk Event Archiver
is installed.
To run:
  1. Select
    Start
    Rockwell Software
    Batch Service Manager
    .
  2. On the
    FactoryTalk Batch Service Manager
    dialog box, choose
    Select Computer
    .
  3. On the
    Select Computer
    dialog box, select the name of the computer where the Archiver Service is installed, and then select
    OK
    . The
    Select Computer
    dialog box closes.
  4. From the
    Service
    list, select
    FactoryTalk Event Archiver
    .
  5. Select
    Start
    to start the
    FactoryTalk Event Archiver
    Service and then select
    Close
    .
    Event Archiver
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal