Configure FactoryTalk Archiver for End of Batch archiving

To use End of-Batch archiving, disable the Archiver Service so that
FactoryTalk Event Archiver
runs as a program triggered by the
FactoryTalk Batch
Server. Use these instructions to disable the Archiver Service.
TIP:
When using End of Batch archiving, the
FactoryTalk Batch
Server's user account must have login access to the Batch History database on the
SQL Server
and the account must have permission to insert and execute data into the BHBatchHis table in the BatchHistoryEx database table.
To configure for End of Batch archiving:
  1. Navigate to
    Services
    .
  2. From the
    Services
    list, double-click
    FactoryTalk Event Archiver
    . The
    FactoryTalk Event Archiver Properties (Local Computer)
    dialog box opens to the
    General
    tab.
  3. From the
    Startup Type
    list, select
    Disabled
    .
  4. Select
    OK
    , and then close the
    Services
    dialog box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal