Archque.txt file

The archive queue file,
ArchQue.txt
, contains a list of electronic batch record files. The line format within the list has the path and file name of the batch record file. The path name can use either UNC names, or local path names. The names depend on the definition of the journal project directory in the
FactoryTalk® Administration Console
in the
FactoryTalk® Batch
Services Properties dialog.
To configure the location used by
FactoryTalk Batch
for storage of event journal files, and the Archque.txt file, open the
FactoryTalk Administration Console
. If you need to add a new server, right-click an application or area where you want to add a server to archive and select
Add New Server
FactoryTalk Batch Server
. Then, right-click the new server, or an existing server, and select
Properties
to open the
FactoryTalk Batch Services Properties
dialog. Select the
Project Settings
tab. In the
Server Directories
area of this tab, go to
Project Directories
and select the browse button next to
Event Journal
or
Duplicate Journal
.
If a batch is removed from the batch list, a tab character (\t) and the word REMOVED follows the file name. Each electronic batch record file is listed in a single record delimited with Carriage Return / Line Feed (CR/LF).
TIP:
Keep the
ArchQue.txt
file locked while it is open and keep it open for only a few seconds. When the queue file is open for more than a few seconds, the
FactoryTalk Batch
Server cannot add entries to the queue as other control recipes are created.
TIP:
The
Archiver queue file
is not written if the
Archive method
is set to
No Archiving - No Queue
. This setting is located on the
FactoryTalk Batch Services Properties
dialog on the
Batch Reporting
tab.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal