Operation Sequence report
The Operation Sequence report displays the association and Operation Sequence data for
FactoryTalk Batch
and SequenceManager
events. This report includes a header section and the Associated Operation Sequences and
Associated Operation Sequences - Details tables. The header displays the specifics of the
batch, such as:Header name | For FactoryTalk Batch, displays | For SequenceManager, displays |
|---|---|---|
Batch ID | Batch ID | Sequence ID |
Unique ID | FactoryTalk Batch Unique ID | SequenceManager Unique ID |
Recipe Name | Recipe Name | Sequence Name |
Area Name | Area | Controller Serial Number |
Process Cell | Process Cell | Controller Serial Number |
Product Code | Product Code | Blank for SequenceManager |
Product Description | Procedure Description | Extended Text |
Completion State | — | — |
Start Time | — | — |
End Time | — | — |
Duration | — | — |
Associated Operation Sequences
For each associated Operation Sequence ID, select the Yellow Tag
to open the Batch Summary report. See the
Batch Summary
report
for more information.Version
The version of the FactoryTalk Batch report provides the following information:
- When the report was last modified.
- The version of the report that is currently installed.
- If a custom report is based on a particular version of a report, it shows which version of the report was used.
Hyperlinks
This report has hyperlinks to these reports:
Icon | Destination Report |
|---|---|
White Tag | Batch Listing |
Yellow Tag | Batch Summary |
White Arrow | Backward Tracing |
Clock | Batch Execution |
Filters
This report features filters for the following:
Filter name | Description |
|---|---|
Start Time | Filters based on start time. Select NULL to filter from the beginning of collected time. |
End Time | Filters based on end time. Select NULL to filter to the end of collected time. |
Batch ID Filter | Accepts search criteria in the form of a Batch Name . Use the asterisk (*) as a wildcard character. |
Process Cell | Filters based on the process cell name or controller serial number. |
Recipe Name | Filters based on the recipe name or the sequence name. |
Unit Name | Filters based on the unit name or the sequence unit ID. |
Unique ID | Specifies which records display in the report. |
Area Name | Users can select all areas or a specific Batch server area name. |
Provide Feedback